(1)| 9/30/2016 12:34 AM | |
|
Joined: 3/6/2012 Last visit: 10/29/2025 Posts: 155 Rating:
|
A GH180 Perfect Harmony medium voltage drive interface has been developed for the iba high speed data acquisition system. No configuration or setup is necessary on the drive side with up to 90 signals trended per drive. 50ms sampling and no additional hardware required. All drives sit on the same trend window for load sharing analysis etc. A very powerful tool for commissioning, fault finding, performance monitoring etc on the Harmony drives. Sample dat file and iba Analyzer software can be downloaded from link below https://www.dropbox.com/s/iqc30p16fu58nft/ibaSiMVD.zip?dl=0 |
|
www.chbdrives.com |
|
This contribution was helpful to
|
|
| 9/30/2016 12:53 PM | |
|
Joined: 3/6/2012 Last visit: 10/29/2025 Posts: 155 Rating:
|
Hi Motorek, The data is available both in live or historical form. To see the live trends you use the ibaPDA software. Have a look around the iba site to get more information on ibaPDA and other products such as HD server which can all be used together with the GH180 interface. The manuals and documentation for this interface will be available shortly with the interface part number being 80.004180. Sampling is set to 50ms as it is all Ethernet based acquisition hence no requirement for extra hardware as we use the standard Ethernet port of the NXGII single board computer. All you need is the IP address of the drives you are connecting to. Once you use this software you will wonder how you ever did work without it. AttachmentInterface-SiMVD_v1.1.pdf (1339 Downloads) |
Last edited by: will4 at: 10/4/2016 4:02:49 AMManual attached. www.chbdrives.com |
|
| 5/19/2017 5:46 AM | |
|
Joined: 3/6/2012 Last visit: 10/29/2025 Posts: 155 Rating:
|
This software now has the ability to acquire the drive data between 10 and 50ms. Supports NXGI, NXGII and NXGpro controllers. AttachmentInterface-SiMVD_v1.2.pdf (1288 Downloads) |
|
www.chbdrives.com |
|
| 6/8/2017 5:34 AM | |
|
Joined: 3/6/2012 Last visit: 10/29/2025 Posts: 155 Rating:
|
Hi Peter, Contact your local iba office http://www.iba-ag.com/en/contact/ibaworldwide/ They will be able to provide you with a quotation. A demonstration of the software or trail licence can also be organised. |
|
www.chbdrives.com |
|
This contribution was helpful to
|
|
Follow us on