(2)| 10/9/2016 5:21 AM | |
|
Posts: 13 Rating:
|
Hi, I am working with step7 ,but I dont know how to use SFC14 and SFC15 for send and recieve data when i have profibus device .can i ask to show me how to use it i need example project .i searche in this from ,i found link of some project but i couldnt open them,please help me ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/10/2016 3:49:11 PMNew subject after splitting |
|
| 10/9/2016 6:31 AM | |
|
Posts: 8092 Rating:
|
Please visit this link. |
This contribution was helpful to
|
|
| 10/10/2016 8:53 AM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear User,
The most straight-forward example that I can suggest would be the following link.It is easy,simple and you can find extra explanations in supporting links.Please read the following FAQ carefully and check the provided STEP 7 project : DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3Pleas note that you need to extract project before opening it with STEP 7. I hope it helps, hdhosseini |
This contribution was helpful to
|
|
| 10/11/2016 5:27 AM | |
|
Posts: 13 Rating:
|
Hi , Thank you for your time, I want to connect to simicode pro (through profidbus).I got gsd file ,and I attached the hwconfig, however i dont know how to read and write ,I dont know i should use sfc58 or sfc 14,15, which one i should use and how can i use it. Thank you again
|
| 10/11/2016 9:02 AM | |
|
Joined: 7/9/2015 Last visit: 1/15/2026 Posts: 4496 Rating:
|
Hi, please check this FAQ: How do you read consistent data from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?Regards, Towome |
|
|
|
Follow us on