(4)| 10/17/2016 9:43 AM | |
|
Posts: 5225 Rating:
|
Helmut_13 - Thank you for the note. Perhaps a more direct link is in order?.. |
| 10/18/2016 12:13 AM | |
|
Joined: 10/26/2013 Last visit: 5/17/2025 Posts: 63 Rating:
|
Is there a changelog? |
| 10/18/2016 3:52 PM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
Start LOGO! Soft Comfort V 8.0 as an administrator. Then Help> Update Center. Select Internet as source. Accept the suggested Internet address "http://www.siemens.com/logo-update". Select the service pack for V8.1 and follow the instructions. |
| 10/18/2016 9:23 PM | |
|
Joined: 10/26/2013 Last visit: 5/17/2025 Posts: 63 Rating:
|
I have found the changelog in the latest 8.1 manual. AttachmentLOGO! 8.1 Soft Comfort Online-help 2016_07 pages 14+15.pdf (3228 Downloads) |
| 10/19/2016 7:12 AM | |
|
Posts: 124 Rating:
|
Hello, I downloaded V 8.1 as follows: Step 1. Doing nothing with actual version installed. No exclusion, no erasion, no nothing. Step 2. Going to the Download page. Link below or posted by William. Same target. Step 3. Downloading according Operation System and platform, and including Java. No ChangeLog was necessary or asked during or after the download. Results: I have now two softwares installed. The old and the new one: V8.0 and V8.1. See picture. Advantage: I have old version with some language and V8.1 in English. If you want to change the language Siemens says: For the installation of language files or the Service Pack, please use the "Update Center" within the Help menu of LOGO! Soft Comfort. Warning: I tried to dowload a language pack but Logo SoftConfort showed a message "Found not information......." I am asking Siemens for a help. A don't receive an answer at a moment. AttachmentUpgrading Logo SoftComfort to V8 1 version 19 10 2016.zip (3698 Downloads) |
Last edited by: Dinos at: 10/19/2016 7:17:55 AMLast edited by: Dinos at: 10/19/2016 7:19:38 AM |
|
This contribution was helpful to
|
|
| 10/19/2016 7:36 AM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
The LSC V8.1 online help provides the following:
Since now all existing language packs are automatically installed and there is no further update, the update center can not find any updates and therefore the error message (or rather to the hint) comes. AttachmentLOGO! 8 Soft Comfort Online-help 2016_07 (FS4) page 15.pdf (1592 Downloads) |
| 10/20/2016 7:58 AM | |
|
Posts: 124 Rating:
|
Hello, The problem about language packs is that V8.1 does not bring the same options as V 8.0. In this case, many users will lost these language possibilities: Czech, Hungarian and Portuguese I am waiting for a answer from Siemens if these languages pack are definetely discontinued. The fact is the number of languagens are been reduced. Regards, |
Last edited by: Dinos at: 10/20/2016 8:26:35 AM |
|
Follow us on