(0)| 10/19/2016 9:35 AM | |
|
Joined: 10/10/2012 Last visit: 1/5/2026 Posts: 22 Rating:
|
Is there any information somewhere on the Siemens area when FS: 05 will start to get delivered when ordering a new S7-12xx? We make modular media transport and sorting systems in series production with each module controlled by a S7-1214, so we would need to migrate, test and release new versions of our PLC programs for F/W 4.2. So far we could just delay that requirement to a point fitting our release plan as we could always downgrade new received CPUs to the latest F/W version tested. Obviously we do not have this option when Siemens starts to deliver FS: 05 ... Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/19/2016 4:23:18 PMNew subject after splitting |
|
| 10/19/2016 11:59 AM | |
|
Joined: 5/12/2006 Last visit: 1/22/2026 Posts: 22807 Rating:
|
Hello, can you say which S7-1214 exactly ? which order number? Regards Christoph |
| 10/19/2016 1:38 PM | |
|
Joined: 5/12/2006 Last visit: 1/22/2026 Posts: 22807 Rating:
|
Hi, i want to know the order number for the 1214 with FS 04 which was delivered to user swen@bibliotheca i know the FS 01 - 03 for the S71214C(DC/DC/DC) or FS03 for S1214FC (DC/DC/DC)but not the FS 04, so i want to know which PLC 1214C he get with a FS 04 and which FW is stored on it.
Christoph |
Last edited by: ChristophD at: 10/19/2016 1:38:40 PM |
|
Follow us on