(0)| 11/3/2016 1:29 PM | |
|
Joined: 1/2/2014 Last visit: 1/11/2026 Posts: 3 Rating:
|
Hi, We are converting a Micromaster vector drive into micromaster 440 which is controlled via USS communication. After changing to micromaster 440,we have found that the drive isn't receiving main setpoint via USS. I have checked that the parameter P2018 receive word 1 is always 0. I am using following communication settings. PZD to 2 and PKW to 3 words. When I tried to change the PKW length to 4 or 127, communication fails. it only works at PKW 3words. Does PKW word length have any influence on the PZD communication in USS? I can receive the control word1 and send 2 words (status word 1 & Actual frequency), but I can't receive the man setpoint via USS. Please help. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/4/2016 9:17:53 AMNew subject after splitting |
|
| 11/3/2016 2:49 PM | |
|
Posts: 8092 Rating:
|
Please check the values of P2012 & 2013 |
| 6/3/2020 9:03 AM | |
|
Posts: 1 Rating:
|
Hi venky_7 did you solve this problem ? if yes tell me how ?
|
Follow us on