(0)| 11/7/2016 2:16 PM | |
|
Joined: 12/3/2010 Last visit: 1/12/2026 Posts: 30 Rating:
|
Hello, I want to “zero” a scale on a siwarex WP522. I tried to use the commands used by siemens in their example.Siemens Example But for some reason it doesn’t work. The SiwarexDB tells CMD2 is finished OK, but my scale is not set “zero” Does anyone has any suggestions? Thanks in advance, Marco |
| 11/9/2016 2:53 PM | |
|
Joined: 12/3/2010 Last visit: 1/12/2026 Posts: 30 Rating:
|
Hi Siwarex, I’m not on the site at this time, so I cannot check if it does work with Siwatool… For some reason I’m getting a finishedError right now and no finishedOK anymore. I expect changes in DR30 or maybe in S_IO_Data. But nothing changes. What else can I check? The only thing I do is Set the trigger bit and write the value 1001 to the CMD CODE. Marco |
Follow us on