(0)| 11/19/2016 12:16 PM | |
|
Posts: 3 Rating:
|
Hello everybody, I have tthe following configuration: 10 inverters Double Motor Module 3 x 3 A each, fed together through a fuse 100 A from the DC bus. The inverters are controlled by a CU 320-2DP. In the CU, everything is "Ready for operation" for all the inverters; howevver, when connecting the infeed, the fuse 100 A blows out. PS. Using the Condenser formation circtuit (3 electric bulbs + 1 circuit breaker), on each inverter everrything is OK. I welcome any suggestions! Thank you in advance, Gheorghe Bogdan ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/21/2016 2:32:35 PMNew subject after splitting |
|
Follow us on