11/22/2016 8:58 PM | |
Joined: 8/25/2014 Last visit: 5/12/2025 Posts: 135 Rating:
|
Hello, all. I'm also having problems establishing the first connection to the LOGO 8! pure. I've read the above described suggestions but it does not work. I can't even ping the Logo which is strange... Also i think that it's strange that if I go to the properties of the PC in network view, the options to set how the IP address is acquiered are greyed out. The option use the following Ip address is checked but it's not the actual IP address of the PC. Could this be the problem??? Cheers. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/24/2016 2:40:39 PMNew subject after splitting |
|
Follow us on