(0)| 11/29/2016 8:31 PM | |
|
Posts: 1 Rating:
|
Hi everyone, I have a very simple and basic doubt. In the datasheet of PS307, 5A and 10A Power Supplies, The Rated input current value is 1.3A and 1.8A respectively at 230VAC. However, in Manual, Siemens recommends to use MCB of rating 10A for each. My doubt is, if it is a SMPS, then why do we need to connect 10A of MCB in the Mains Line? A simple 3A MCB will do the same job. Isn't it? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2016 1:45:16 PMNew subject after splitting |
|
| 11/30/2016 2:35 PM | |
|
Posts: 4620 Rating:
|
Hello, perhaps for inrush startup? |
Follow us on