(1)| 2/15/2017 4:48 PM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36500 Rating:
|
There are two different hardware versions of the LOGO! 0BA8. The older one is 0BA8.Standard. It has the Fimverwareversionen V1.08.01 to V1.08.03 (corresponds to the production stands FS01 to FS03). With the LOGO! Soft Comfort V8.0.x, only programs for the 0BA8.Standard can be created and edited, but not for the 0BA8! .FS4. For the correct upgrading also the V8.1 please see this topic: Upgrading from LSC V8.0 to LSC V8.1 Edit: For upgrading start the LSC V8 as an Administrator. |
Last edited by: ixo65 at: 2/15/2017 4:49:59 PM |
|
This contribution was helpful to
|
|
| 2/15/2017 4:55 PM | |
|
Posts: 158 Rating:
|
I re-opened as administrator and it loaded....THANK YOU |
Last edited by: markheuer at: 2/15/2017 4:57:59 PM |
|
This contribution was helpful to
|
|
| 2/15/2017 5:02 PM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36500 Rating:
|
I also updated many times, and I never had a problem. Also not with the upgrading fom V8.0 to V8.1. There you can go another way: Download from this Siemens Website Demo software , upgrades/updates, Drivers the upgrade-file, it is a "Setup.exe" file. After downloading run the Setup.exe as an Administrator. |
| 7/26/2017 8:11 AM | |
|
Posts: 8171 Rating:
|
New question published by gustavosa is split to a separate thread with the subject Is it possible to create a file in a SD card to load into old version firmware v1.08.03 with LSC 8.1 and new LOGO?. Best regards |
Follow us on