(0)| 2/2/2017 1:55 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36484 Rating:
|
One possibility is to store the counter reading by means of an arithmetic instruction. |
| 2/2/2017 2:24 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36484 Rating:
|
In german Forum there is a nice program from User Betel, dim with one push button. Take a lot a this, it the last post in the topic. Download the file "DEMO_1_tastenbedienung Dimmen V4 (0BA6).zip". Hoch/Runter dimmen mit 1 Taster: Anzahl der Schritte |
| 2/3/2017 7:19 AM | |
|
Posts: 6 Rating:
|
Hi ixo65, I've managed to get 85% of it working with a work around (basically I change the counters "ON" value with the different scenes). It's not fully working, however I'm getting closer. At the moment the program looks a bit messy due to the testing, but if you (or someone else) has some time to check whether they might have a better solution for it? It would be appreciated. Also perhaps someone else can use parts of this program for their own use. If someone manages to get a better version to work, please repost AttachmentLight Control TEST.zip (471 Downloads) |
| 2/3/2017 5:04 PM | |
|
Posts: 65 Rating:
|
I already had to do something like this, where you could set light output, stored in a counter using the Logo front panel keys. Using a timer block I wanted to load the counter with a preset value, a night time value in my case. The circuit basically either increments or decrements the counters value to the preset value. Change the async pulse generators values to control how quickly the counter increments/decrements. Attached is the relevant section from my design. AttachmentIncrementing Counter.zip (533 Downloads) |
| 8/22/2017 7:40 AM | |
|
Posts: 8171 Rating:
|
New question published by mark.boere is split to a separate thread with the subject Fixed value will continuouslly be written to the device - Which solution is the best?. Best regards |
Follow us on