4/17/2017 5:13 PM | |
Posts: 1 Rating:
|
Dear all Genious, I have faced a problem with s7 200 PLC. I have a old plc with a program by another programmer. In that program he used I0.0 for read pulses from a inductive sensor. but he didn"t use HSC. he use only two timer and a MOV command like below I0.0 >> ----I I-------[T120] with +200 ms I0.0 >> ----I/I-------[T121] with +200 ms T120 >> ----I I---------------------------[MOV +0 VW890] I T121 I ------I I------------------ anybody pls help me. how can it possible ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/18/2017 7:47:58 AMNew subject after splitting Last edited by: Min_Moderator at: 4/18/2017 7:48:34 AMContact data deleted |
|
Follow us on