(0)| 4/15/2017 11:53 AM | |
|
Joined: 8/9/2011 Last visit: 10/8/2025 Posts: 325 Rating:
|
Hi , I have a Hardware configuration - CPU 226 CN with module Ethernet CP (CP 243-1) + wincc flexible 2008 sp3 for runtime I am facing a problem of communication resulting #### on runtime . Problem remains untill the PLC is not power cycled. But after few minutes the problem repeats. All the cables and ethernet switch used are confirmed to be Okay Online I have checked the condition Cable loss . If i reconnect the cable properly also problem remains as long as PLC is not power cycled. But if i manually disconnct and connect back the cable wen everything ok , the communication re-establishes normally. Pls check the attachment. Waiting for the solution. ------------------------------------------------------------------------------------------ |
Last edited by: GaJEnDrA D S at: 4/17/2017 4:25:55 AMLast edited by: Min_Moderator at: 4/18/2017 3:53:58 PMNew subject after splitting "Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
| 4/19/2017 9:05 AM | |
|
Joined: 4/24/2006 Last visit: 1/14/2026 Posts: 9105 Rating:
|
Hello, Perhaps the following links might help: Best regards, Wizard |
Follow us on