(6)| 4/21/2017 4:43 PM | |
|
Posts: 2826 Rating:
|
Hello. An earlier discussion lead to the discovery (thanks Alex Mol). Further investigation was done to compensate for this. I need it for an active project. The findings and SCL code are now shared for discussion.
Attachmentstopwatch code.zip (814 Downloads) |
Last edited by: #dP at: 4/21/2017 4:54:23 PMLast edited by: #dP at: 4/21/2017 4:55:08 PMLast edited by: #dP at: 4/25/2017 5:07:46 PM |
|
This contribution was helpful to
|
|
| 5/5/2017 6:10 PM | |
|
Posts: 2826 Rating:
|
Hello Alex. Now THAT is what I call teamwork! So this is how open-source projects look like. Thank you for pushing through with the test. Nicely done. Good results too. The ca. 3ms gap can probably be explained if one looked at the structure of the test code. it is too strange that it is in the ballpark of the cycle time. Attached is the code segment that contains the improved #OVERFLOW value. Some extra (boring?) notes have been added into the code that explains what was done. So - - - - - - what is next? AttachmentStopWatch_V2.zip (803 Downloads) |
This contribution was helpful to
|
|
Follow us on