(0)| 4/24/2017 3:57 PM | |
|
Posts: 59 Rating:
|
I tried a project with CPU 314 with SM331 ai 8x13BIT 6ES7 331-1KF02-0AB0 through TIA V13 SP 1 or 2. Although the AI module is showing ok (green) in the hardware configuration, it (IW; not accepting PIW tag) is showing always online zero value with different analog voltage or resistance input. Please proide information whether TIA V13 can be used for this AI module. I tried the same with S7 V5.5 and it is working with only PIW tag although it is not showing error with IW tag. Then I tried to migrate the S7 V5.5 project file to TIA V13 SP2 but failed due to the message " S7 V5.4 SP5 or V5.5 is not installed". As I installed TIA V13 SP2 first, it is not allowing to install S7 V5.4 or 5.5 in the same laptop. I have installed S7 V.5 in another laptop. Is there any way to solve the above migration problem other than re-installation of S7 V.5 first and TIA V13 SP2? Please advise solution of the AI module programming using LD language. Thanks Mr. ChristophD. I have solved the problem of using IW for analog input at TIA V13,
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/25/2017 11:20:02 AMNew subject after splitting Last edited by: fiah at: 4/26/2017 6:11:24 AMLast edited by: fiah at: 4/26/2017 4:35:23 PM |
|
Follow us on