(0)| 4/19/2017 11:56 PM | |
|
Joined: 4/3/2017 Last visit: 1/17/2026 Posts: 69 Rating:
|
Thank you for everything! I will put zip file of my project, it is made in LogoSoft 7 and i downloaded LOGO! app on my android device...I connect two of my LOGOS which are in MASTER/MASTE(client) configuration but in CONTROL PAGE of app i can't make button which can change my for example input 1 in MASTER logo.. I dont know how to configure Target Tag, what VB or VW should i use and how? I also want to make slader for analog input for MASTER(client) logo.. I don't know how to configure all that things in app or should i change something in my programs.. Have you any idea what can i do, just to control something? P.S. file called Kraj.isc is for MASTER logo and file krajclient.isc is for MASTER(client) logo ------------------------------------------------------------------------------------------ AttachmentLOGO APP.zip (337 Downloads) |
Last edited by: Min_Moderator at: 5/2/2017 8:23:27 AMNew subject after splitting |
|
| 4/20/2017 5:57 AM | |
|
Joined: 12/18/2014 Last visit: 1/22/2026 Posts: 36503 Rating:
|
Do you know this manual? https://support.industry.siemens.com/cs/document/109486018/logo!-logo!-app-v-10?dti=0&lc=en-WW |
| 5/2/2017 6:09 AM | |
|
Joined: 12/18/2014 Last visit: 1/22/2026 Posts: 36503 Rating:
|
The constant X is used only to terminate open output "legs" of digtal blocks. X has nothing to do with the VM memory. If you want to transfer the state of an input to a partner device, it only goes over the VM area. The constant X has nothing to do with it. Either make it with an input byte IB or use a network output instead of the constant X. However, the LOGO! 0BA7 network outputs only to a slave LOGO! send. A VB is a byte in the VM area. It can be used both for digital purposes and for analog purposes. I have not written that the IB0 or VB0 contain I1 to I7. I wrote the following:
Except there is no IB0.0. There is only one IB0, IB1 and IB2. AttachmentLOGO! 8 Soft Comfort Online-Help english sides 105-109 (vm range).pdf (466 Downloads) |
Last edited by: ixo65 at: 5/2/2017 6:15:06 AMattachment |
|
Follow us on