(1)| 5/16/2017 8:33 PM | |
|
Joined: 1/1/2017 Last visit: 10/30/2025 Posts: 343 Rating:
|
Dear All, I've provided the addressing as per standard only but still the CPU integrated Inputs are not responding! Can anybody suggest what may be the probable reason for this issue! I'm forcing the values in VAT table, the changes are responding in logic, but when physically I'm providing external 24VDC to the channels they are not responding in the logic! Please help me. Regards Omkris ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/17/2017 12:11:33 PMNew subject after splitting |
|
| 5/23/2017 1:22 PM | |
|
Posts: 623 Rating:
|
Hi, What is the status of input LEDs? Please check wiring as per CPU manual. |
| 6/1/2017 11:51 AM | |
|
Joined: 2/11/2015 Last visit: 1/8/2026 Posts: 515 Rating:
|
try to not wire the outputs and force agains the output, the LED is lighting?¿ |
Follow us on