(0)| 6/29/2017 8:57 AM | |
|
Posts: 9 Rating:
|
Hi friends I want to communicate one master and four slave CPU of 1214c ac/dc/relay type (all CPU are of same type) and i have done with the communication between two CPU but third one is not communication properly so kindly suggest me the sample program for this thanks & regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/30/2017 10:02:58 AMNew subject after splitting |
|
| 6/30/2017 12:21 PM | |
|
Posts: 9 Rating:
|
sir CPU is 1214c ac/dc/relay communication is by siemens green TCP/IP cable all CPU are of same type modle number is 6ES7-214-1BG40-0XB0 |
| 6/30/2017 12:46 PM | |
|
Posts: 9 Rating:
|
sir, I have tried it with GET/PUT as well as TSEND_C/ TRCV_C it is helpful only for communication between two CPU |
| 6/30/2017 1:01 PM | |
|
Posts: 9 Rating:
|
Yes i am using siemens green TCP/IP (profinet) cable |
| 6/30/2017 2:51 PM | |
|
Posts: 5521 Rating:
|
hi abdul, try this: Configuration and application of PROFINET I-Device function this would be the easiest way to communicate whit the requirements you have. hope this helps, regards, |
| 7/1/2017 7:26 AM | |
|
Posts: 9 Rating:
|
Sir, kindly send me the sample program for that if possible |
Follow us on