7/16/2017 11:22 PM | |
Posts: 15 Rating:
|
Did you configure a DNS Server for the IOT2000? Seems the address couldnt be resolved. |
7/17/2017 5:30 AM | |
Joined: 2/27/2014 Last visit: 8/28/2025 Posts: 689 Rating:
|
Hello, Hope you are able to access internet via X2 port which is dhcp enable. Then you need to do some security setting in your gmail account to send and receive email via IoT2040. Allowing less secure apps to access your accountGoogle may block sign-in attempts from some apps or devices that do not use modern security standards. Since these apps and devices are easier to break into, blocking them helps keep your account safe. Some examples of apps that do not support the latest security standards include:
Change account access for less secure appsTo help keep G Suite users' accounts secure, we may block less secure apps from accessing G Suite accounts. As a G Suite user, you will see a "Password incorrect" error when trying to sign in. If this is the case, you have two options:
If you still can't sign in to your account, the"password incorrect" errormight be caused by a different reason |
With Best Regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on