(0)| 8/8/2017 11:58 AM | |
|
Posts: 9 Rating:
|
Hi Guys I'm new here. Currently working on a simple startup project. My system consists of S7 1214 DC/DC/DC connected to DC 24 V power supply. (6ES7 214-1AE30-0XB0) I'm trying to make the simplest program work: A simple push button input to energize one output. Problem is when I connect power to the digital input, nothing happens! The corresponding LED lights up but nothing on the output side. - I connected all M contacts to DV- and 3L (on output rail) to DV+ - Using I1.1 as input to get Q0.5 output - When I enable monitoring, I also don't see any action in my network (Network 1, Ladder environment) - Address of I/O starts from I0.0/Q0.0 in hardware configuration, so the addresses I used must be valid and not out of range I think I'm missing something here! Please help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/9/2017 11:32:18 AMNew subject after splitting |
|
Follow us on