7/28/2017 10:10 AM | |
Joined: 7/26/2017 Last visit: 10/8/2023 Posts: 13 Rating:
|
For Torque control what should I have to vary voltage or current? same for speed control? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/10/2017 10:26:21 AMNew subject after splitting |
|
7/28/2017 5:31 PM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating:
|
|
7/30/2017 6:49 PM | |
Joined: 7/26/2017 Last visit: 10/8/2023 Posts: 13 Rating:
|
In which mode use in this programme? I mean torque or speed control? |
7/31/2017 9:48 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating:
|
If you need just drill machine equipped with "Start/Stop" buttons and "Speed" potentiometer. I think there is not necessity to use Sinamcs VFD,which offers more far capability you need.Of course more capability means that more money you should pay. So I think you have to pay attention to younger brother of Sinamics, it's MICROMASTER. As example look at this variant: 6SE64402UC155AA1
Using Starter you can select Configuration -> Wizard - Speed Control (encoderless) for motor settings. |
Last edited by: Msorich at: 7/31/2017 9:53:54 AMLast edited by: Msorich at: 7/31/2017 10:36:20 AM |
|
7/31/2017 10:14 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating:
|
To youre selected anologue input you need to configure following as shown below. |
7/31/2017 11:03 AM | |
Joined: 3/31/2015 Last visit: 7/30/2025 Posts: 175 Rating:
|
Please do not recommend MICROMASTER 4 as a younger brother of SINAMICS. MICROMASTER 4 is soon to be phased out. Also, if I read it correctly and the motor is a single phase motor please see: https://support.industry.siemens.com/cs/document/12519917/ And get a 3 ph motor |
Last edited by: m_zlotek at: 7/31/2017 11:06:14 AMLast edited by: m_zlotek at: 7/31/2017 11:06:30 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on