(0)| 9/13/2017 8:23 AM | |
|
Posts: 15 Rating:
|
DEAR EXPERT We are facing problem at out one straightening and cutting m/c. in our steel plant during commissioning period . At time of commissioning sensor module of one motor (SENSOR MODULE INT20 , 6SL3055-OAAOO-5MAO 5193004002. VERSION B ) was broken , and system was showing drive fault , after then we don't get same module from siemens .but we got another one is - SENSOR MODULE SM 120 , ASE - 33412837 VERSION P , We fitted at motor and connect communication cable, but drive fault showing again. our system is ---- SINAMICS 120 , CPU 317 - 2DP CONTROL UNIT CU320 , 6SL 3040 OMAOO OAAL SIMOTION D 445 , 6AU1445 - OAAOO - OAAO ACTIVE INTERFACE MODULE , 6SL 3330- 7TE33 8AAO DRIVE - VECTOR CONTROL , S 120 ,6SL 3120 1TE24 - 5AM So my problem is that this new sensor module sm 120 is it suitable or not? , may be fault generated inside CU UNIT and it is need to be reset internally . so how to short out this problem ? can you help us ? , we are suffering from last few month , but still we not get it solution . thanks . Mr. KADAM . Electrical engg. M/S B5 PLUS LTD., GHANA ( WEST AFRICA ) MOB. NO 00233260674213 . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/14/2017 10:16:01 AMNew subject after splitting |
|
| 9/13/2017 11:40 AM | |
|
Joined: 10/11/2006 Last visit: 1/19/2026 Posts: 6069 Rating:
|
Hello, you can find instructions to change a SMI20 in section 12.8 of the function manual FH1 https://support.industry.siemens.com/cs/de/de/view/103498916/en?dl=en |
|
With best regards, |
|
Follow us on