(1)| 12/1/2017 7:38 PM | |
|
Posts: 226 Rating:
|
the days off they do not work .... maybe someone can help in the program ... CTRL_HSC_EXT =does not work does not count pulses CTRL_HSC =OK Attachmenttemp_hsc_1_20171201===.zip (652 Downloads) |
Last edited by: SAR-CNT at: 12/1/2017 7:41:17 PM |
|
| 12/1/2017 10:38 PM | |
|
Posts: 103 Rating:
|
The description in the system manual is a bit thin but seems good enough. The English descriptions of the HSC_Count structure is attached. AttachmentHSC_Count structure.zip (808 Downloads) |
| 12/2/2017 2:24 PM | |
|
Posts: 2826 Rating:
|
Hello.
Yes that is a dreadful situation. As "luck" would have it, I am in the process of transitioning from TIA13 to TIA14. I am spending some time to see what changes are available in TIA V14 SP1 Update 3. Earlier this week I was researching the HSC . Studying the System Manual I found some helpful tips. What you ask is attached as a PDF.. an extract from the manual. There are more information there too. I will only be testing my efforts for a project later the coming week. Any hints you could provide when you test yours, will be most welcome. Regards. Update: Attachmentfiles.zip (587 Downloads) |
Last edited by: #dP at: 12/2/2017 2:30:52 PMLast edited by: Jen_Moderator at: 12/4/2017 7:36:14 AMAdded picture and pdf as an attachment. |
|
This contribution was helpful to
|
|
Follow us on