(0)| 12/16/2017 5:32 PM | |
|
Posts: 1 Rating:
|
Hello, I have a simatic panel tp170b on s7 300 system. I want to back up tp 170b and than load to tp 177b. is it possible ? i |
| 12/16/2017 6:36 PM | |
|
Joined: 3/28/2015 Last visit: 1/4/2026 Posts: 727 Rating:
|
Hello, 1-If the Panel TP 170B "Programmed with Protool Software": You need the Configuration program of the panel then migrate it with WinCC Flexible 2008 SP2 and change the panel type into TP 177B 2-If the Panel TP 170B "Programmed with WinCC Flexible Software": You need the Configuration program of the panel and change the panel type into TP 177B 3-Uploading the Configuration program only possible, if the Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable back transfer". |
|
Eng.Mohamed Ibrahim |
|
| 1/29/2018 2:52 PM | |
|
Posts: 8171 Rating:
|
New question published by plc.giang is split to a separate thread with the subject HMI TP177B do not start Window CE . Best regards |
Follow us on