(0)| 12/22/2017 4:39 PM | |
|
Posts: 2 Rating:
|
I want control and monitor 4 devices DSE8610 with (Wincc Flexible or Wincc7). DSE8610 is a controler for diesel generator that support Modbus TCP and Modbus RTU 485. The problem is this : Wincc does not have COMMUNICATION DRIVER for DSE8610. For monitoring DSE8610, The example in last post from Mr_AWE is very good and applicate. In This example use ''Modicon Modbus TCP '' for driver and "Premium,Micro" for CPU type. For control DSE8610: Control is performed by sending System Control Keys to the module, and also sending the bitwise opposite (or one’s compliment) of the control key to another register ‘in the same write operation’ for security. One of the system control keys must be written into register 4104 and its ones-compliment written into register 4105 with a single function 16 (write multiple registers) to perform the specified system control function. Now i want control DSE but i do not know how send function 16 to DSE. Thanks for your helps. ------------------------------------------------------------------------------------------ Attachment056-051 Gencomm Control Keys.pdf (804 Downloads) |
Last edited by: Ahmad_Ghafari at: 12/22/2017 4:39:57 PMLast edited by: Ahmad_Ghafari at: 12/22/2017 4:43:20 PMLast edited by: Ahmad_Ghafari at: 12/23/2017 3:13:00 PMLast edited by: Jen_Moderator at: 12/26/2017 6:41:04 PMNew subject after splitting |
|
Follow us on