(0)| 12/26/2017 6:29 PM | |
|
Posts: 75 Rating:
|
Hello everybody. D.G. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/26/2017 8:05:14 PMNew subject after splitting |
|
| 12/27/2017 5:26 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Gujaa; It does not matter to WinCC Flexible what mdules are connected to the PLC. You onl;y have to setup a Profibus connection to each of the CPUs through its Profibus address, and collect the tags you need in the WinCC Flexible screens you want to develop. When you say you want to build a SCADA, you mean that you will be using a PC , not an operator panel? In that case you will need a license for WinCC Flexible 2008 SP3 Advanced., and also Runtime (RT) licenses: https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/10018718 See the following documents for information and tutorials on WinCC Flexible 2008 communications:: WinCC flexible 2008 Communication Part 1:see section 2.2.4 https://www.youtube.com/watch?v=-3WpH9MjqPc&list=PL0B9F322B315BCC89 - Complete list of WinCC Flexible tutorials from the same source: https://www.youtube.com/playlist?list=PL8oo40E4ujcrh8HBKL0PitHjwJSki5XvW I suggest you start with one connection to one of your CPUs, and with a few selected tags. When you have done this and you can exchange a few data with one PLC, the rest will be only a question of planning and design, and afdding a second connection to the second CPU. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/27/2017 7:47:09 PMLast edited by: CS Moderator at: 1/7/2018 11:54:39 PMchanged link to a more permanent one |
|
Follow us on