1/29/2018 8:46 AM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
The easiest way to install Java on a single IOT2000 image is running the 32-bit Oracle JRE installer. This seems to work, despite the Quark Erratum. The safest way is letting Yocto recompile OpenJDK for the target processor by integrating meta-java (http://layers.openembedded.org/layerindex/branch/master/layer/meta-java/) into a custom image and adding openjre-8 as additional package, similar to https://support.industry.siemens.com/tf/ww/en/posts/creating-custom-layer/182600/?page=0&pageSize=10. PS: If you reply in Spanish, please make sure google translate can process it again |
2/5/2018 10:35 AM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
If you are not yet familiar with Linux, I would recommend to install the Oracle 32-bit JRE as described in https://java.com/de/download/help/linux_install.xml directly on the running IOT2000. |
1/17/2019 2:49 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, To install Java the way Jan described above, check out this post. Kind regards! |
Follow us on