2/6/2018 12:24 PM | |
Joined: 7/16/2016 Last visit: 1/16/2024 Posts: 28 Rating:
|
Hello I am new with cnc.I work on a cnc machine to change the sinumerik controller(840C) The drives are simodrive 611 (6sn1123).actually I d like to know which sinumerik controllers I can replace with. the control boards of four axis are pulsed control and the other four servo drives controlled by analog signal that coming from plc, Please someone help me how to do that? the name of replacement sinumerik? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/7/2018 10:23:07 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
2/11/2018 4:49 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, You have not provided servo motor & spindle motor details. You need to chcek the type of encoder feed back compitability. You need to chcek the axes configuration in project e.g. no of gemotrical axes configured, no of axes controlled by PLC, need to select NCU etc. etc. However as desired by you please find below here with links of manuals. Please down load & study. SINUMERIK 840D sl Commissioning CNC: NC, PLC, DriveCatalog NC 62: SINUMERIK 840 Equipment for Machine ToolsSINUMERIK 840D sl SINUMERIK Operate (IM9)SINUMERIK 840D sl Detailed Machine Data Description |
Last edited by: Jen_Moderator at: 2/12/2018 10:33:41 AMOptimized links. |
|
Follow us on