(0)| 2/17/2018 3:56 AM | |
|
Posts: 3 Rating:
|
Dear Sir. I need to connetc a PLC S7 1200 with SENTRON PAC5200 using MODBUSTCP. When doy you say: " I changed MB_UNIT_ID= 1 in MB_CLIENT_DB" You refer to CONNECT_ID YOU CAN HELP ME WITH SOME DOCUMENT OF THE MODBUS REGISTER OF THE SENTRON PAC5200 FOR THE PAC3200, in the manual there is the next "Modbus measured variables with the function codes 0x03 and 0x04"; but for the SENTRON PAC5200, Don´t see. I want to thank you, your response Regards. Cristhian ------------------------------------------------------------------------------------------ |
Last edited by: Cristhian22021987 at: 2/17/2018 4:12:51 AMLast edited by: Jen_Moderator at: 2/19/2018 12:34:54 PMNew subject after splitting |
|
| 2/19/2018 1:47 PM | |
|
Posts: 3093 Rating:
|
Communication Manual SENTRON PAC5100/5200 7KM5212/5412 Regards, |
| 2/21/2018 8:33 AM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16661 Rating:
|
Hello Cristhian here is an FAQ perhaps the way of doing is imilar to your device: https://support.industry.siemens.com/cs/ww/en/view/40614428 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 2/22/2018 6:49 PM | |
|
Posts: 3 Rating:
|
Hi Murof I read the manual and it helped me a lot Thanks for the information Regards Cristhian |
This contribution was helpful to
|
|
| 2/22/2018 7:58 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Cristhian; See the following information on the Energy values of the PAC5200. Hope this helps, Daniel Chartier |
Follow us on