(2)| 2/26/2018 6:14 PM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
The CM1241 is a communication module. I don't think it can be used for encoder input. You need something like the PosInput modules:
As far as I know, there is no version for central use with S7-1200. You will need to use a ET200SP (PosInput1) or ST200MP station (PosInput2). An other solution is a PROFINET encoder like 6FX2001-5.N... |
|
|
|
This contribution was helpful to
|
|
| 2/26/2018 6:44 PM | |
|
Joined: 7/7/2010 Last visit: 1/20/2026 Posts: 16386 Rating:
|
You are correct about the CM1241 not being useful for encoder input of the type already purchased and linked above by OP/TS. The DI modules I mentioned can be configured as high speed counter inputs, and collectively for A/A-/B/B- for speed and direction as quadrature encoder input.
|
|
science guy |
|
This contribution was helpful to
|
|
| 1/7/2020 9:55 AM | |
|
Joined: 10/1/2019 Last visit: 7/25/2025 Posts: 1 Rating:
|
Hello, I have a similar problem. I'm making an application using 5 positioning measuerment systems, which work on 5V TTL, so I can't use signal board, because it has only 4 DI. I have a 1214C DC/DC/DC CPU and idea was to read value via 1241 RS422/485 module. Is it even possible to use 1241 module as a high speed counter and to read the value? If it helps I have a Hiwin PM-B-05-0D-G-20-01 measurement system.
|
| 1/9/2020 12:59 PM | |
|
Joined: 8/31/2005 Last visit: 12/16/2025 Posts: 2198 Rating:
|
As I wrote, I think: No RS422 only defines the electrical characteristics (which signal is high, which is low), but not what kind of information is transferred. And the CM1241 provides a serial interface and not a encoder input. |
|
|
|
Follow us on