(2)| 3/8/2018 11:20 AM | |
|
Posts: 224 Rating:
|
Hi I have a HMI (TP1200 Comfort) and a PLC (CPU 1513-1 PN) that I want to connect to a customers network so they can have Remote access using Sm@artServer. I have a LAN cable between PLC port x2 and HMI port x1, so that there is connection between them. Can I just connect my costumers network to PLC port x1 or HMI port x2, and then change the IP-address for both the PLC and HMI so it is the same as my customers network? As far as I can read, both the PLC and HMI have ethernet interface. Best regards |
| 3/12/2018 11:46 AM | |
|
Posts: 8171 Rating:
|
New question published by Azkaban is split to a separate thread with the subject What is the difference between Industrial Ethernet (IE) and ProfiNet?. Best regards |
Follow us on