3/13/2018 9:35 AM | |
Posts: 69 Rating:
|
I am about to commission a ride called MAVERICK at an amusement park. I am not sure which type of braking they are using. Can you please explain on both Hydraulic and pneumatic braking done through drive.? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/14/2018 10:12:28 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
3/13/2018 9:46 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
It depends upon type of brake, is it disck type or cylindrical (the programer needs to study the operation & saftey requirements first). Generaly from your application it is fail safe i.e. when motor is OFF, brake is applied & when motor is ON, brake is released, but better confirm it. Further more DO controls the brake valve operation & brake released positive feed back is configured to drive or controller. Safety is always first priority. You need to check, how drive is controlled, via PLC or any other controller, safety norms must be followed. Please refer DC Converter Application document for functional safety STO, SS1 (ISO 13849-1) manual which will help you to impliment safety instrunctions. HTH. |
Last edited by: Jen_Moderator at: 3/13/2018 2:43:58 PMOptimized link. |
|
3/13/2018 10:08 AM | |
Posts: 69 Rating:
|
It is a hydraulic disc brake. How can I enable the DOs for brake valves? Can you give me a simple example? |
3/14/2018 6:00 AM | |
Posts: 69 Rating:
|
Hello, How to assign joystick functions with dc drive? |
3/15/2018 1:20 PM | |
Posts: 69 Rating:
|
I want to configure a ride's movement UP and Down. How can I use this up and down movements(ie, forward and reverse) using this joystick digital inputs? |
3/20/2018 5:10 PM | |
Posts: 69 Rating:
|
Can I use the two motor drives in one arm in master and slave mode for my application? If yes, how can I do that? |
Follow us on