(3)| 4/12/2018 2:55 PM | |
|
Joined: 2/20/2015 Last visit: 11/19/2025 Posts: 12 Rating:
|
Hi,
Your contribution is confirming what I expected in regard to "when the data is updated". Also I found this FAQ now, saying it's more performant (...transfer commands provides a particularly convenient and high-performance method of access (low runtime load)) to read from the process image. My conclusion is now: If it sufficient in regard to the update time, better read/write from/to the process image instead of using SFC14/15. Btw, we are working with PIPs. The block will be put in OB35 and the PIP is assigned to OB35, too. So the inputs are read before processing OB35 and the outputs are written after processing OB35. We will have a lot of instances and I fear wasting to much processing time, when always reading/writing with SFC14/15. Thanks guys |
This contribution was helpful to
|
|
Follow us on