(0)| 5/15/2018 11:05 AM | |
|
Posts: 146 Rating:
|
Dear colleagues, What happens when tag number is reached? I have a project with MP370 and 2100 Power tags. When I compile project in WinCC Flexible (2008 SP3) I do not get any error message. What will happen when I download this project to MP370 panel, is there going to be some problem because tag number is reached? Milos ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/15/2018 1:36:58 PMNew subject after splitting |
|
| 5/16/2018 5:11 AM | |
|
Joined: 7/5/2013 Last visit: 1/19/2026 Posts: 3275 Rating:
|
Hello Milos,
the Operating Instruction shows on page 1-7 that you can have max. 2048 tagsfor the MP370 (Maximum total number for PowerTags and internal tags). But in some forum statements it sounds like only the "cyclic continuously" tags are counted. In my opinion an error message should be shown after compiling, if you use too many tags, because there is no option to increase the number of powertags as it is possible for the WinCC fexible Runtime. Regards, Frink |
|
Pi is exactly three! |
|
Follow us on