(0)| 5/18/2018 12:08 PM | |
|
Posts: 4 Rating:
|
I'm working with SIPROTEC 7SJ62. After going online with a parameter file having a version number V4.7 and initializing the 7SJ62 device several times while trying different things etc every thing was working well. Then I decided to download a project with a parameter file having a version V4.6 without updated the parameter file to V4.7. I managed to initialize the device and download into the 7SJ62 successful and without any apparent problems. On trying to initialize again with some other projects ( the ones that I was working before) I start having the below massage and unable to initialize the 7SJ62 any further. Any suggestions please? I have attached also the fault file which should be sent to the DIGSI hotline ( but I do not have a clue how to contact them) AttachmentErrorBuf.txt (806 Downloads) |
| 5/18/2018 12:09 PM | |
|
Posts: 4 Rating:
|
|
| 5/18/2018 1:36 PM | |
|
Posts: 108 Rating:
|
You can reset under voltage trip via menu in device. Control-tagging-set-block U<. |
This contribution was helpful to
|
|
| 5/18/2018 2:14 PM | |
|
Posts: 4 Rating:
|
Thanks mate .. This solved the problem |
Follow us on