(0)| 5/23/2018 11:33 AM | |
|
Posts: 52 Rating:
|
Hello Sirs, I have the same problem. After 5 seconds, the STO signal is activated. The signals SS1 & SLS functions are de-activated. The material I use is a CU250S-2 PN with a PLC S7-1511F. (And license memory card for Safery Integrated Extended functions 6SL3054-7TE00-2BA0 Z-F01) Telegram 30 & 352 I have observed that if during these 5 seconds I start the drive, it works correctly and the SLS and SSM functions work well. I have the same missing enables: bit 0 OFF1 enable missing bit 8 Safety enable misisng bit 17 OFF2 enable internal missing bit 30 speed controller inhibited Regars ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 5/23/2018 1:28:34 PMNew subject after splitting |
|
| 5/24/2018 8:50 AM | |
|
Joined: 10/11/2006 Last visit: 1/21/2026 Posts: 6072 Rating:
|
Hello, |
|
With best regards, |
|
Follow us on