(0)| 9/4/2018 8:13 AM | |
|
Joined: 4/28/2015 Last visit: 1/19/2026 Posts: 402 Rating:
|
Hello, is your used encoder really suitable for this module? The supported encoder/signal types are:
Maybe it is usefull to have a look at the manuals: Equipment Manual "SIMATIC ET 200SP TM PosInput 1" Function Manual "SIMATIC S7-1500, ET 200MP, ET 200SP Counting, measurement and position detecti" If TM POSINPUT is not the right module for your application, please have a look at the TM COUNT module, wich supports the following encoder/signal types:
ET 200SP, TM Count 1x24V Equipment Manual "SIMATIC ET 200SP TM Count 1x24V" |
Follow us on