(0)| 9/24/2018 7:33 AM | |
|
Posts: 14 Rating:
|
Good day, experts! When I try to connect to the Sinamics DCM 6RA8093-4GS22-0AA0-Z, the following message "SSP not installed..." (look at screen). |
| 9/24/2018 7:34 AM | |
|
Posts: 14 Rating:
|
На ПК установлены Starter V4.4 и SSP Sinamics DCM V1.4 SP1 (посмотрите на экран) В чем может быть проблема? Помоги мне, пожалуйста. Спасибо! |
| 9/25/2018 5:12 AM | |
|
Posts: 14 Rating:
|
Hello friends! Can someone help me? Look posts 1 and 4. Thank you! |
| 9/27/2018 9:56 AM | |
|
Posts: 14 Rating:
|
Good day experts! Is there no solution to my problem and no one can help me? |
| 9/28/2018 6:28 AM | |
|
Posts: 8092 Rating:
|
Hello, Please refer attached file which will help you to establsih communication between PC & 6RA80 drive with STARTER via RS232. Also from your 1st post, your installed Starter software needs update & requires SSP. It can be downloaded by Siemens employees only. So please contact your nearest Siemens support center. Please refer this link for more details. Firmware for the SINAMICS DCM / SINAMICS DCM Control Module and the associated SSPs for STARTER - News (refer STARTER SSP) HTH Attachment6RA80 Starter RS232 communication.pdf (593 Downloads) |
Last edited by: PISCEAN 2010 at: 9/28/2018 6:35:33 AMLast edited by: PISCEAN 2010 at: 9/28/2018 6:36:53 AM |
|
| 9/28/2018 7:44 AM | |
|
Posts: 8092 Rating:
|
What error is displayed? Have you set PG/PC interfacing paramerts & sinamics DCM parameters correctly? |
Follow us on