(0)| 9/24/2018 4:41 PM | |
|
Joined: 1/27/2016 Last visit: 9/24/2025 Posts: 7 Rating:
|
Dear Expert, I am in commissioning of one G150 12-pulse infeed. Before changing P860, everything is OK and contactors are activated and drive is started. According to attached manual, I changed P860 from r863.1 to r722.5, but when i start the drive no command sent to contactors (from CIM) obviously no contactors feedback signal received and F7300 appeared. I don't know why command of contactors not issued and which parameter is related to command of line contactors. Regards, AttachmentSINAMICS_G150_Converter_Cabinet_Units_en-US_2016.pdf (264 Downloads) |
Follow us on