(0)| 9/27/2018 8:40 AM | |
|
Joined: 10/19/2016 Last visit: 7/11/2025 Posts: 316 Rating:
|
Good morning, I have a test bench used for testing some simple mechanical device such as rotary table, electrospindle, ecc... here's the configuration: SINUMERIK; 840D sl; NCU 710.3BPN with PLC 317-3PN/DP Software CNC, 4.7 SP4, CF with license 6SL3121-1TE31-3AA3 SMM 6SL3055-0AA00-5BA3 SMC20 I would to understand how to commission a simple torque motor connected with an encoder EnDat2.2 without STARTER. Siince i don't have an updated electrical scheme, another possibility would be the one of a self-recognition of the system. Attached the pdf with errors.
AttachmentBinder2.pdf (308 Downloads) |
|
𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
| 9/28/2018 12:42 PM | |
|
Posts: 8092 Rating:
|
Please refer manual SINUMERIK 840D sl Commissioning CNC: NC, PLC, Drive chapter 6.8 |
| 9/29/2018 9:14 AM | |
|
Posts: 8092 Rating:
|
Hello, Please check if encoder connections are connected correctly & for SMC40 follow below steps correctly. (you need to connect encoder to SMC & then only possible to configure topology. During the initial commissioning, you must absolutely observe the following rules: 1.Connect at least one of the DRIVE-CLiQ interfaces X500/1 or X500/2 on the SMC40 using DRIVE-CLiQ. 2. Connect one EnDat encoder to the corresponding encoder interface X520/1 (to X500/1) or X520/2 (to X500/2). 3. Operate the SMC40 only in a star topology. The DRIVE-CLiQ X500/1 and X500/2 sockets cannot be used for a series connection. HTH Please check www.heidenhain.de/connectivity_endat22_drive-cliq link to confirm compatibility / connection issue of Heidenhain encoder with SMC40. |
Last edited by: PISCEAN 2010 at: 9/29/2018 10:09:25 AMLink added |
|
Follow us on