3/29/2019 6:00 AM | |
Joined: 8/2/2018 Last visit: 8/17/2025 Posts: 10 Rating:
|
Hi Pls find the files to load 3.4 & instructions. Regards Sanjaya Srivastava AttachmentLoading FirmwareCUVC.pdf (563 Downloads) |
Regards |
|
This contribution was helpful to
1 thankful Users |
4/1/2019 8:42 PM | |
Posts: 5 Rating:
|
Hi Its a T300 with a TSY 2.52 rom The preliminary file I load is MASTERDRIVES VC(CUVC)_tm I have attached the file Thanks for your reply Regards Mike AttachmentMASTERDRIVES VC(CUVC)_tm.doc (468 Downloads) |
Last edited by: Mikes2016 at: 4/1/2019 9:11:05 PM |
|
4/2/2019 1:41 AM | |
Posts: 5 Rating:
|
Hi I am working to a set of instructions supplied by one of our support contractors and learning as I go.I suspect the answer will be get on to our live working drive and do a complete upload. Step one is to load MASTERDRIVES VC(CUVC)_tm.doc into drive monitor Followed by many steps of modifying parameters then file - download - save to eprom RSD_C_Standard_CUVC (attached) The drive goes into F116 before I get to this stage at a point where I Change P060 to 7 Goes into a Device identification request. "A technology board has been detected but no technology type has been configured." and options to generate a data base. Thanks for the reply AttachmentRSD_C_Standard_CUVC.doc (399 Downloads) |
Last edited by: Mikes2016 at: 4/2/2019 2:02:55 AM |
|
4/2/2019 11:13 PM | |
Posts: 27 Rating:
|
Hello mikes. reset the drive to the factory setting. and setting up again |
Follow us on