(0)| 4/11/2019 10:20 AM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello No, if you only run the WInCC Advanced RT on the PC then you do not need to use the Station Configuration. You can only run and load the HMI Runtime (only if you have special hardware or if you use Simatic Net devices like Simatic NEt OPC Server or Softwarebased PLCs then you need it). Here is the very basic FAQ for this Topic: https://support.industry.siemens.com/cs/de/en/view/89852595 If you want to connect a Classic Simatic Manager Project then you can use this one: https://support.industry.siemens.com/cs/de/en/view/73502293 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on