(0)| 6/24/2019 1:06 PM | |
|
Joined: 12/12/2016 Last visit: 12/11/2025 Posts: 640 Rating:
|
Hello, Are you using the latest SDK (V2.4.0)? Some project settings have to be changed because the Eclipse plugin has not been updated yet. Check out this thread. Also make sure that you run 7-zip 16.04 as Admin when you extract the files. Kind regards! |
| 6/24/2019 1:40 PM | |
|
Joined: 4/17/2019 Last visit: 11/10/2025 Posts: 21 Rating:
|
I changed the settings like it's explained in that thread. I also use the right version of 7-zip. in the screenshot you can see that there are less errors. But when i build the project, the same error occurs on the console. |
Follow us on