(0)| 11/17/2008 6:33 PM | |
|
Posts: 11 Rating:
|
Hi, Please find attached screen dump of one of my applications which uses the cursor keys to increment/decrement two counters which in turn are used toadjust the setpoint of two timers. These timers are then used to set an output energsied for shotdose duration time after interval duration time has elapsed (i.e. act as an adjustablerecycle timer). Hopefully this clarifies use of the cursor keys. Best regards, Corby AttachmentUsing cursor keys to adjust counter.pdf (4160 Downloads) |
| 11/18/2008 10:17 AM | |
|
Posts: 661 Rating:
|
Try not to press ESC + C at the same time but first ESC and hold it. Then the C. |
| 11/24/2008 11:14 PM | |
|
Posts: 4 Rating:
|
Hello CorbyLee Thank you for answer, but have you ever try this? Please try to use kursor key and you will see my problem. Best Regards BrOs |
| 11/25/2008 5:50 PM | |
|
Posts: 4 Rating:
|
Hello Fux, Here is a part of my program. Input I2 is instead of pulse at the midnight. With cursor keys I want to adjust START and STOP time, when output Q1 have to be active. Because of easy testing I put minutes instead of hours and seconds instead of minutes. Best Regards BrOs AttachmentTimer_01.zip (1602 Downloads) |
Follow us on