1/4/2021 12:17 PM | |
Joined: 12/31/2020 Last visit: 6/24/2022 Posts: 3 Rating:
|
I have a SIEMENS LOGO PLC! 8 6ed1052-1cc08-0ba0 24CE programmed to store in the SD memory the data connected to an analog input. I want to know if it is possible to access the SD through the LOGO ACCESS TOOL and see the historical data in Excel program. I've installed the complement "LOGO! access tool" in Excel, but when I try to access into the PLC by IP address the Excel program reports "error 91 at run time". I am using MS Office professional plus 2010. ---------------------------- |
Last edited by: CS Moderator at: 01/04/2021 13:23:07New subject after splitting |
|
1/4/2021 2:38 PM | |
Joined: 12/18/2014 Last visit: 9/21/2025 Posts: 36023 Rating:
|
No, the Access Tool cannot access the SD card directly, only the variable that is to be logged. |
1/11/2021 6:51 PM | |
Joined: 12/18/2014 Last visit: 9/21/2025 Posts: 36023 Rating:
|
I don't know ... May you can ask Siemens. Start a Support Request. |
Follow us on