(0)| 9/12/2021 2:02 PM | |
|
Posts: 6 Rating:
|
Hi Chris, Surely there are some methods to do so. I am about to write a paper to explain how to do that step by step. But I am busy and it takes time to do so. As a short answer: 1- First you need to learn to work with NCVAR Selector. You need to purchase this software or use PG with the Sinumerik toolbox installed. 2- Then you need to read the 611D Drive manual very well to be familiar with all parameters you can extract from your Drive MD 3- You are required to use a gateway to convert Profibus to Ethernet. - usually, the MPI port is occupied and Profibus is empty but if both are occupied, you need a repeater I have tested this brand: Helmholz 4- Next step is programming PLC and setting DBs for FB2 function (SIMODRIVE 611 digital/SINUMERIK 840D/810D Drive Functions Function Manual 2010) 5- Final Step is to use a SCADA software to log, archive, and combine all parameters in a meaningful way Each step requires much more detail. If you have no problem with the budget, you can go for "Softing uaGate 840D" and skip all steps above except the first and second one. If I had time to publish my article about the step-by-step procedures, I will let you know. Yours, Kaveh Izadi |
| 9/16/2021 9:29 PM | |
|
Joined: 4/28/2015 Last visit: 1/17/2026 Posts: 387 Rating:
|
Hi Nulizhang, Yes the gateway supports 840D Powerline along with some third party controllers - please see the flyer attachment. Hope this helps Luke AttachmentBrownfield_Connectivity_Services_Flyer_EN (1).pdf (793 Downloads) |
Follow us on