(1)| 6/9/2021 7:46 PM | |
|
Joined: 2/17/2020 Last visit: 1/15/2026 Posts: 1251 Rating:
|
Hi SummerSeaSun, The first thing I would check is the compatibility between WinCC 7.5 (including ServicePack and Updates if any) and the operating system of the PC on which it is installed. If you have a Server-Client architecture, I would check compatibility with all the PCs involved. To do this: Welcome to the compatibility tool On the other hand, I would check if the PC meets the minimum system requirements to work with WinCC, in case it is low on RAM, for example. Finally, perhaps the DCF file is causing problems, as indicated in the following FAQ: Why does the screen change in WinCC V7 projects suddenly slow down by up to several seconds? I hope that helps. |
|
A rating will be well appreciated. |
|
This contribution was helpful to
|
|
| 6/10/2021 11:28 AM | |
|
Joined: 2/5/2013 Last visit: 1/14/2026 Posts: 345 Rating:
|
Solved the issue on the original project deleting PRT folder! Thanks to all, BR |
| 6/10/2021 3:02 PM | |
|
Joined: 2/17/2020 Last visit: 1/15/2026 Posts: 1251 Rating:
|
Great! Thanks for letting us know! |
|
A rating will be well appreciated. |
|
Follow us on