(0)| 12/7/2021 8:15 AM | |
|
Posts: 50 Rating:
|
Dear Experts, We have purchased both DCM Drive . I have enclosed here for DCM drive name plate . Pls remove txt in my attachment find the image on the drive rar file name plate...... Pls confirm this both drive having inbuild Profinet communication . Thanks In advance, Regards, AttachmentDCM Drive Manual.rar.txt (696 Downloads) |
| 12/7/2021 9:15 AM | |
|
Posts: 8092 Rating:
|
Hello, Could not open attachment. Why don't you combine snap shot of nameplate files in zip folder & attach? |
| 12/7/2021 9:27 AM | |
|
Joined: 12/18/2014 Last visit: 1/21/2026 Posts: 36503 Rating:
|
Here's the same as ZIP file ...
AttachmentDCM Drive Manual.zip (691 Downloads) |
This contribution was helpful to
|
|
| 12/7/2021 9:50 AM | |
|
Posts: 8092 Rating:
|
Hello Puli Kutty, 6RA8018-6DV62-0AA0 is basic 4Q 25A DC drive. 6RA8031-6DV62-0AA0 is basic 4Q 125 A DC drive. To connect Profinet, user need to go for advanced CUD unit + profinet module which is option. Please check the convenient location of installation of advanced CUD in drive & then user can order left or right advanced CUD along with Profinet board. Hope this helps. |
Follow us on