(1)| 6/30/2009 12:34 PM | |
|
Posts: 5 Rating:
|
Everytime the drive go in operating mode appear the current fault warning W5001 power unit chip over temperature. I think that this is just only noise of signal because if I check the parameter signal r37.1 with the trace (attacced starter trace) I can se the temperature start from 30°C to over 120 °C in just only 0,7 seconds and after go down. This is not possible really!! The ambient temperature is 30°C and the cooling fan is working. Can the p290have some influence? All sinamics drives in this plant have the same kind of problem.
Thanks Attachmentwarning 5001.zip (504 Downloads) |
Last edited by: Simone-EDM at: 6/30/2009 12:38 PM |
|
| 6/30/2009 12:47 PM | |
|
Posts: 5 Rating:
|
the issue is possibile see on parameter r37.1 |
| 7/1/2009 3:47 PM | |
|
Joined: 9/18/2006 Last visit: 1/21/2026 Posts: 596 Rating:
|
Hi. Excuse me, but I have not understood *.trc Best regards. |
| 7/17/2009 2:48 PM | |
|
Posts: 5 Rating:
|
I'm using SINAMICS S120 CM 6SL3720-1TG37-4AA0-Z |
Follow us on