(6)| 3/25/2010 1:55 AM | |
|
Joined: 7/1/2008 Last visit: 6/8/2025 Posts: 15 Rating:
|
Dear Mich See the attached file & do the Wincc flexible Communication connection settings, it will work. IN HMI addressput your Computer IP address In PLC address put your PLC simulator IP address Also note that the both IP address are in same Series Like 192.168.10.xx (PLC)--> 192.168.10.xx (PC). AttachmentPLCsim.pdf (3571 Downloads) |
This contribution was helpful to
|
|
| 3/25/2010 4:25 PM | |
|
Posts: 29 Rating:
|
I was setting the TCP/IP adress 192.168.10.3 and then RUN the HMI interface but don´t compile because there is a ERROR with the parameters. Please help me |
| 9/30/2010 2:32 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello Look at attachment. Just start PLCSIM (change connection to PLCSIM(PROFIBUS)), start runtime in WinCC Flex... To open attached project, you will need at least Step7 is 5.4 + SP4 and WinCC Flex is 2008 SP1 + HF2 Best regards, Hristo Mihalev AttachmentSample.zip (1863 Downloads) |
Last edited by: UMENCHO at: 10/8/2010 11:32 AM |
|
This contribution was helpful to
|
|
| 6/21/2011 6:47 PM | |
|
Joined: 6/14/2011 Last visit: 4/5/2025 Posts: 20 Rating:
|
Thank you so much |
This contribution was helpful to
|
|
Follow us on